Technical FAQs

Ask a Question

Is a toggle extension needed for the H or J frame breaker when used with a 9422CSF50?

Yes, the extension should be included with the op mech kit The individual part number is 29904-11540

CTA-ID : 2053684
Was this helpful?
What can we do to improve the information ?