Technical FAQs

Ask a Question

Is there a DIN rail mount for a REG48PUN2LJLU temperature sensor?

There is no DIN rail adapter for the 48 X 48mm sensor. It will have to be panel mounted. We only have a DIN rail adapter for the 24 X 48mm units. It is part number REG24PSOC.


CTA-ID : 2053916
Was this helpful?
What can we do to improve the information ?