Technical FAQs

Ask a Question

How can I use the Altivar 61/71Daisy Chain topology? Modbus TCP/IP Ethernet daisy chain card. If the cards are daisy chained and the first and last drive on the network is connected to a switch, the customer says it is bringing the network down.

If the Ethernet card VW3A3310D is daisy chained and the two drives at the end of the network is connected to a switch, the switch must be managed with RSTP or hypering enabled.


CTA-ID : 2053822
Was this helpful?
What can we do to improve the information ?