Technical FAQs

Ask a Question

What size bolts are used on the YA2500R7?<br />

1/2-13 x 2` bolts are used with the RLTB adapter.


CTA-ID : 2053805
Was this helpful?
What can we do to improve the information ?