Technical FAQs

Ask a Question

What is the correct position nomenclature for the motor cutoff switch for HVL/cc switches.

If the motor cutoff switch is in the on position, the motor is connected.

If the motor cutoff switch is in the off position, the motor is disconnected.


CTA-ID : 2053795
Was this helpful?
What can we do to improve the information ?