Technical FAQs

Ask a Question

What are the derating factors for a Motorpact lineup installed at 2200 Meters Elevation?

If the system will have properly selected surge (lightning) arresters per ANSI C37.010 standard, it is not necessary to derate the system. If no arresters are used then the derating factors in the standards must be used.


CTA-ID : 2053902
Was this helpful?
What can we do to improve the information ?