Technical FAQs

Ask a Question

Are expander lugs available for NEMA type contactors and starters to increase the size and quantity of wire feeding the line side?

NEMA starters have available only the lugs sizes they are designed with. Replacement lugs are available, but not optional lugs for larger size cables.

CTA-ID : 2053555
Was this helpful?
What can we do to improve the information ?