Technical FAQs

Ask a Question

What material are the meter jaws on an EZML114225 made from?

The meter jaws on EZM products are made of tin plated copper with a tension spring to hold the jaws together on the meter terminal.

CTA-ID : 2053584
Was this helpful?
What can we do to improve the information ?