Technical FAQs

Ask a Question

What is the difference between the regular and super duty PFC Capacitors found in Digest 175 page 4-29?

The super duty type use higher voltage rated capacitors. They have higher voltage withstand, and also a higher temperature rating than the units with the regular duty rating.


CTA-ID : 2053560
Was this helpful?
What can we do to improve the information ?