Technical FAQs

Ask a Question

Is it possible to order an I Line panel with a 400A main breaker and 400A branch breaker with a Kirk Key interlock installed interlocking the 2 breakers?

Issue:
Is it possible to order an I Line panel with a  400A main breaker and 400A branch breaker with a Kirk Key interlock installed interlocking the 2 breakers?

Product Line:
I line panelboards.

Environment:
Products sold in the United States.

Cause:
Availability.

Resolution:
Yes. This can be done with a Main Lug Only panel with two branch mounted breakers mounted side by side. It cannot be done when the main breaker is vertical mount.


CTA-ID : 2053536
Was this helpful?
What can we do to improve the information ?