Technical FAQs

Ask a Question

Can you use a GFI (Ground fault interrupt) on a 115V single phase input with a ATV11 drive?

The PWM in the drive can cause problems with the GFI, because of the capacitance to ground. It is not recommend to use a GFI with the drive.
If a GFI have to be used, then suggest installing an isolation transformer between the GFI and the drive. Also the motor needs to be properly grounded.

CTA-ID : 2053249
Was this helpful?
What can we do to improve the information ?