Technical FAQs

Ask a Question

On a SDSB1175C surge suppression unit what size breaker do we recommend?

To protect an SDSB1175C, the application must use a 15-30 ampere rated breaker, because the connecting wire must be also protected.


CTA-ID : 2053054
Was this helpful?
What can we do to improve the information ?