Technical FAQs

Ask a Question

What are the part numbers for the HCM48TS 4 piece trim?<br /><br />

The top and bottom is part number 80104-890-01 and the two side pieces are part number 80104-891-01.



CTA-ID : 2053344
Was this helpful?
What can we do to improve the information ?