Technical FAQs

Ask a Question

What is suffix PLILC on a QO115 and QO120 breaker?

It provides a load shedding feature for breakers used in a QO intelligent load center. The breakers will shut off when the power goes out so that they are not being used on generator power and will turn back on when the power is restored.

CTA-ID : 2053259
Was this helpful?
What can we do to improve the information ?