Technical FAQs

Ask a Question

Will a QO2L30S accept QOB breakers?

Issue:
Will a QO2L30S accept QOB breakers?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
QO load centers are designed to accept only plug-on QO circuit breakers. They are not designed to accept bolt-on QOB circuit breakers. If QOB bolt-on breakers are required, consider using a NQ panelboard.


CTA-ID : 2053251
Was this helpful?
What can we do to improve the information ?