Technical FAQs

Ask a Question

Does the DJ Mission Critical breaker have the same ratings as the other DJ breakers? Is it adjustable?

It has the same ratings. Ir (long time) is adjustable; ST and Inst. are preset and not adjustable.


CTA-ID : 2053431
Was this helpful?
What can we do to improve the information ?