Technical FAQs

Ask a Question

How big a padlock will the MG26970 take? <br /><br />

The MG26970 allows the IEC C60 circuit breaker to be locked in either the ON or the OFF position (UL 489 Listed and UL 1077 Recognized devices can lock in the OFF position only). The padlock attachment accepts a 0.315 in. (8 mm) diameter padlock, which is not supplied.

CTA-ID : 2053383
Was this helpful?
What can we do to improve the information ?