Technical FAQs

Ask a Question

What is the difference between the logic reed contact block 9001KA41 and the power reed contact block, 9001KA51?

Issue:
What is the difference between the logic reed contact block 9001KA41 and the power reed contact block, 9001KA51?

Product Line:
Harmony Push Buttons

Environment:
Harmony 30mm

Cause:
Product Specifications

Resolution:
The 9001KA41 is rated for 1/2 amp continuous current, the 9001KA51 is rated for 3 amp continuous current.


CTA-ID : 2053436
Was this helpful?
What can we do to improve the information ?