Technical FAQs

Ask a Question

Can aluminum wiring be used with 8502, 8536, 8538, 8539 and other NEMA Starters?

The wire that should be used in the copper lugs is `Solid or stranded copper wire`.


CTA-ID : 2053446
Was this helpful?
What can we do to improve the information ?