Technical FAQs

Ask a Question

Is there an additional mounting kit to mount a PBQ3640G on a horizontal run?

No.  A horizontal busway application does not require a mounting kit accessory.
But a horizontal mounted unit should be independantly supported with threaded rods to the ceiling. Contractor is responsible for the threaded rods.

The vertical busway application requires an additional mounting kit PBQ4060RMK.



CTA-ID : 2053258
Was this helpful?
What can we do to improve the information ?