Technical FAQs

Ask a Question

What is the arm and roller material on the 9007T/FT made of ?

The roller arms are die cast zinc construction with hardened, oil impregnated, sintered iron rollers.


CTA-ID : 2053278
Was this helpful?
What can we do to improve the information ?