Technical FAQs

Ask a Question

Can DC breakers such as catalog number KHL3625025DC be used on AC applications?

No. These breakers are strictly designed and UL marked and listed for use on DC circuits only. Specifically designed for use on UPS systems.

CTA-ID : 2053274
Was this helpful?
What can we do to improve the information ?