Technical FAQs

Ask a Question

What is the part number for a 8940WD3S2 external reset?

The complete, door mounted, external reset mechanism assembly requires the following parts:
Qty 1 - 30019-113-59 - Reset sub-assembly (does not include the ring nut or gasket listed below).
Qty 1 - 30019-121-01 - Ring nut.
Qty 1 - 29206-30700 - Gasket.


CTA-ID : 2053110
Was this helpful?
What can we do to improve the information ?