Technical FAQs

Ask a Question

Is there a replacement for the XALD144 keyed selector switch control station?

Catalog number XALD144 is a non-domestic product, not available in the USA. However, one can be built by using the following domestically available components: XALD01 enclosure, ZBY2178 legend plate, ZENL1111 contact block, ZB5AG2 keyed operator.

CTA-ID : 2053338
Was this helpful?
What can we do to improve the information ?