Technical FAQs

Ask a Question

What is the continuous current rating on an H366 heavy duty fusible safety switch?

The continuous current rating of a fusible safety switch is dependent upon the ampacity of the fuses installed and the type of load that the switch is feeding. The National Electrical Code regulates the sizing of overcurrent protection based on the type of load. Typically, but not always, the overcurrent protection will be sized at 125% of the full load current.


CTA-ID : 2053165
Was this helpful?
What can we do to improve the information ?