Technical FAQs

Ask a Question

What is the AIC rating of the HCN14654M panelboard? What is the catalog number of the main breaker?

The main breaker is an LAP36400, which is rated at 42K at 240V, 30K at 480V, or 22K at 600V, which would be the highest fully rated AIC rating level of the HCN14654M panelboard.


CTA-ID : 2053129
Was this helpful?
What can we do to improve the information ?