Technical FAQs

Ask a Question

What are the NEMA and IP enclosure ratings for the 9007T and 9007FT type of limit switches?

The 9007T and FT limit switches are: NEMA 1,2,4,12,13, and also IP65, IP66, and IP67.

CTA-ID : 2052127
Was this helpful?
What can we do to improve the information ?