Technical FAQs

Ask a Question

What are the dimensions of the standard circuit directory card for NQOD and NF panelboards catalog number 80031-158-01?

Issue:
What are the dimensions of the standard circuit directory card for NQOD and NF panelboards catalog number 80031-158-01?

Product Line:
Panelboards.

Environment:
Product selection.

Cause:
Product features.

Resolution:
The card is approx. 5 1/2`` X 5 1/2`` square.


CTA-ID : 2052403
Was this helpful?
What can we do to improve the information ?