Technical FAQs

Ask a Question

What is the part number for the base that the light module attaches to on a 900KP pilot light?<br />

3105404201 is the base part of a pilot light. This is the 9001KP with no ring nut, gaskets, thrust washer, etc.

CTA-ID : 2052345
Was this helpful?
What can we do to improve the information ?