Technical FAQs

Ask a Question

Will a QE3200VH breaker series rate with a QO breaker?<br />

No, the QE3200VH is currently obsolete and no longer available and was used in older style EZM equipment. The QE3200VH breakers will not series rate with QO breakers today, because QO breakers and load centers today are not marked or UL listetd with series ratings for QE type breakers.

CTA-ID : 2052134
Was this helpful?
What can we do to improve the information ?