Technical FAQs

Ask a Question

Was there ever a circuit breaker with a gray handle?

Yes, the FH, KH, LH, MH breakers used to have gray handles. Also back when the standard QO breakers had a 5,000 A.I.C. rating the QH , 65000 A.I.C. rated breakers had gray handles.

CTA-ID : 2052186
Was this helpful?
What can we do to improve the information ?