Technical FAQs

Ask a Question

Is a Nema 3R Model 6 motor control center available in a reduced height?

Issue:
Product Features


Product Line:
Motor Control Centers

Environment:
NEMA ICS 18-2001, EEMAC, UL 845, NFPA70 Art. 430

Cause:
To clear overhead obstructions reduced height may be necessary.

Resolution:
There is no offering for a reduced height, NEMA 3R enclosed Model 6 motor control center.


CTA-ID : 2052075
Was this helpful?
What can we do to improve the information ?