Technical FAQs

Ask a Question

Can the incandescent bulb in 9001 light module be swapped out with a LED bulb?

We don`t offer different voltage LED lamps in the 9001`s in all the voltages. We use either 6 or 12 volt LED in the 9001KM light modules. These light modules have resistors so that no matter what the input is we get 6 or 12 volts on the output. If the unit is a transformer light module, we do have 6 volt lamps. However the transformer light modules for the LED`s are not the same as the transformers for incandescent lamps. The light output of the LED might not be what they want.


CTA-ID : 2052286
Was this helpful?
What can we do to improve the information ?