Technical FAQs

Ask a Question

Are the NQ panelboard rail extension assemblies ,usable in both NEMA 1 and NEMA 3R enclosures?

Issue:
Are the NQ panelboard  rail extension assemblies ,usable in both NEMA 1 and NEMA 3R enclosures?

 Product Line:
NQ Panelboard

Environment:
Maintenance

Cause:
Ordering

Resolution:
Yes. All rail extension kits are usable in both the NEMA 1 indoor and NEMA 3R weatherproof enclosures.


CTA-ID : 2052289
Was this helpful?
What can we do to improve the information ?