Technical FAQs

Ask a Question

What are replacement lugs for a CK1200N (35030)?

46960 which is a set of 3 lugs which each accepts (4) #4/0 to 500kcmil cables per lug or 46966 which is a set of 3 lugs which each accepts (3) 250 to 600 kcmil cables per lug. Both are obsolete without replacement.


CTA-ID : 2052769
Was this helpful?
What can we do to improve the information ?