Technical FAQs

Ask a Question

What is the maximum number of auxiliary contacts on a NEMA Size 1 Starter?

You can add up to qty (5) auxiliary contacts. These will consist of up to qty (4) external and qty (1) internal auxiliary contacts in addition to the normally open holding circuit contact provided as standard.


CTA-ID : 2052402
Was this helpful?
What can we do to improve the information ?