Technical FAQs

Ask a Question

400V 50hz Short Circuit Ratings and Continuous Bus Ratings

Per MCC Design Engineering, 480V 60Hz LVMCC bus withstand ratings will also be valid at 400V, 50hz. The same can be said for continuous current ratings of the LVMCC bus system.

CTA-ID : 2052660
Was this helpful?
What can we do to improve the information ?