Technical FAQs

Ask a Question

What is the actual terminal data on the GS1AW406?

The GS1AW406 will accept up to 12 conductors : Torque varies by wire size

6﾿4 35 lb-in
8 25 lb-in
12﾿10 20 lb-in



CTA-ID : 2052119
Was this helpful?
What can we do to improve the information ?