Technical FAQs

Ask a Question

When opening the front panel on a Mini PowerZone transformer (e.g. MPZB15T2F) the brackets and hinges keeping the door open bends slightly. Are the components strong enough to allow the panel to remain in the open position?

When opening the door you will have to slide the door back a bit and maneuver it until the grooves seat into the sheet metal. The door might sag slightly when in the open position, but it is fine and will stay open.


CTA-ID : 2052560
Was this helpful?
What can we do to improve the information ?