Technical FAQs

Ask a Question

What is the wire range of the PK27GTA equipment ground bar terminals?


Product Line:
LC Accessory

Terminal wire range

The PK27GTA has 27 terminals that accept (1) #14 - #4 or (2) #14 - #12 AWG copper wires or (1) #12 - #4 or (2) #12 - #10 AWG aluminum wires. It is also supplied with a lug that accepts (1) #6 - 2/0 AWG copper or aluminum wire. This lug is packaged loose and is not attached to the 27 terminal ground bar. If the 2/0 lug is field installed onto the ground bar, the number of smaller terminals will be reduced to either 25 (if the lug is mounted at the end of the ground bar) or 24 (if the lug is mounted in positions other than at the end of the ground bar).

CTA-ID : 2052428
Was this helpful?
What can we do to improve the information ?