Technical FAQs

Ask a Question

Can a thermal imagery be used to get readings on a safety switch through a viewing window?

No, the Viewing Window doesn`t give line of sight viewing of all the lugs and fuse clips that could also be over heating. It`s main purpose is to show that the blades are open. Therefore, the VW feature is not recommended for thermal sensing tactics.

CTA-ID : 2052151
Was this helpful?
What can we do to improve the information ?