Technical FAQs

Ask a Question

What is the part number for the Nema 3 and 4 handle assembly for the Powerpact M and P frame breaker?

The painted Nema type 3 and 4 handle assembly is a 9421LHP48. The chrome plated Nema 3, 4 and 4x handle assembly is a 9421LCP48.

CTA-ID : 2052430
Was this helpful?
What can we do to improve the information ?