Technical FAQs

Ask a Question

Customer was having trouble mounting a PQ3603G?

There are 2 hanger hooks on the back of the switch. The hanger hook on the right side of the unit (above the handle) is positioned in the busway slot at the top right of the plug-in opening. Engage the left hook over the entire duct top flange. (The left hook is not required to be positioned in the busway slot to the left of the plug-in opening.)

CTA-ID : 2052339
Was this helpful?
What can we do to improve the information ?