Technical FAQs

Ask a Question

What is the AIC rating of the HD and JD frame breakers used in I-Line panels when used at 250 VDC? Normal AIC at that DC voltage is 20K. Product selectors is rating the I-Line DC panels at 18K

The UL maximum DC rating on these breakers when used in I-Line panels is actually 18K, not 20K. This is a standard level for UL testing.

CTA-ID : 2052303
Was this helpful?
What can we do to improve the information ?