Technical FAQs

Ask a Question

What is the wire range of the lugs provided on the UTH4330T individual meter socket?

Issue:
Wiring

Product Line:
Meter Socket

Cause:
Terminal lug data

Resolution:
The UTH4330T meter socket is shipped standard with incoming and outgoing Line, Load, and Neutral studs only (lugs not included), and the lugs are to be ordered separately and installed in the field. Six lugs will be required (one each for the incoming and outgoing line, load and neutral studs). Depending on the job and local utility requirements, there are two appropriate lug kits:
ARP00129 - includes one, single barrel lug for #4 AWG - 600 kcmil (al/cu)
ARP00427 - includes three, two barrel lugs for #6 AWG - 350 kcmil (al/cu)
 
Was this helpful?
What can we do to improve the information ?