Technical FAQs

Ask a Question

What is the part number of the roller arm only for an XCKL115?<br /><br />

Arm is available with the head. Order ZCKD15. It may also be ordered separately as ZCKY15


CTA-ID : 2052205
Was this helpful?
What can we do to improve the information ?