Technical FAQs

Ask a Question

Is the 82355R Double throw switch suitable for use as service equipment?

Product Design Features

Product Line:
Double Throw Safety Switches



Yes, the 82355R is Suitable for use as Service Equipment. BUT per the NEC and depending on the application, it will either require a Ground kit or a Solid Neutral Assembly.

Note: Typically, if used on a 3PH/3W voltage system, use the PKOGTA2 ground kit. If used on a 3PH/4W voltage system, install solid neutral assembly DT400N.

CTA-ID : 2052940
Was this helpful?
What can we do to improve the information ?