Technical FAQs

Ask a Question

What legend plates are used with the XACB pendant stations?<br />

The old style ZB2BY**** 30mm X 40mm plastic legends are used with the XACB pendant stations. See Digest 175 page 19-116 for available legends.


CTA-ID : 2052924
Was this helpful?
What can we do to improve the information ?