Technical FAQs

Ask a Question

Can an MAL breaker be converted to an MAP?

Yes, but only if the following conditions are met. If the lugs are removed from the on end of the MAL breaker, it must be secured with pan-mounting screws, or have ﾿P﾿ screws (cover screws and nuts) installed securing the base to the cover.

CTA-ID : 2052888
Was this helpful?
What can we do to improve the information ?