Technical FAQs

Ask a Question

What size power fuse clips are used on a size 2 starter unit at 480V?<br />

60A fuse clips.
Class R fuse clips require qty. (3) 153034 and qty. (1) 80409-423-50.
Class H fuse clips require qty. (3) 153034 and qty. (1) 40512-411-50
Class J fuse clips require qty. (3) 153034 and qty. (1) 40512-411-50


CTA-ID : 2052033
Was this helpful?
What can we do to improve the information ?